STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 361 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 287 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

RNG1 probe error: Configuration incorrectly allows both A7S and A7NS to be selected simultaneously

We're using the ST v5.0 eco-system and v.6.9 of STM32CubeMX.Per RNG internal peripheral - stm32mpu, the RNG1 peripheral should be a single choice assignment. When I click on A7S (OP-TEE), the tool warns me that it cannot be removed from the A7S conte...

SLivi.1 by Associate II
  • 3857 Views
  • 4 replies
  • 2 kudos

Resolved! DDR_Init_A7 unable run

DearsI can only start this example in Debug mode, the BLUE led start blinking... So it works OK.But If I try to use RUN command (using icon, or right mouse click on project file) than it seems not work (RED leds blinks only ONE and is OFF, Blue LED i...

ravo by Senior
  • 2940 Views
  • 4 replies
  • 1 kudos

STM32CubeProgrammer on STM32MP153CAB3

Dear Support and Experts Need your kindly help to advise. I am currently designing programming station to program STM32MP153 on a panel consist of 6 identical boards with command line utility. Kindly advise.1. Whether STM32CubeProgrammer is a right p...

sdonsri by Associate
  • 1060 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP13 empty STM32Cube project "hello world"

HelloCan I use Windows and STM32CubeIDE to develop application using STM32MP135FAF7 (STM32MP135F-DK discovery kit).I tried to create empty project based on this discovery kit but it ended with message"This project requires OpenSTLinux version 'openst...

ravo by Senior
  • 3622 Views
  • 6 replies
  • 2 kudos

STM32CubeProgrammer on STM32MP153

Dear Experts Need your kindly help to advise. I am designing programming station to program STM32MP153 on a panel consist of 6x identical boards with command line utility. Kindly advise.1. Whether STM32CubeProgrammer is a right programmer for this pa...

sdonsri by Associate
  • 1065 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 1.14.1 released

Hello, Since the STM32CubeIDE 1.14.0 release, some issues was faced when executing shell script in the pre/post build command. This issue was faced with the Windows version of the STM32CubeDE 1.14.0. Therefore, a patch is now available on ST site whi...