User Activity

I am trying to build a custom board for the stm32mp151A using the STM32MP15 Evaluation boards as a reference.U-BOOT starts, but the kernel won't start, and I'm at my wit's end.1. When the device starts up, the console displays "CPU: STM32MP151AAC Rev...
 When I add a debug log to the source code, a [version-going-backwards] error occurs.  ERROR: weston-cube-4.0+gitAUTOINC+cd44839e95-r0 do_packagedata_setscene: QA Issue: Package version for package weston-cube went backwards which would break package...
Custom STM32MP151A board with 512MB DDR2.I am trying to write via UART communication with STM32CubeProgrammer, but BL32 processing does not start.What should I do to investigate the cause? [2024-01-12 14:11:52.591] NOTICE: CPU: STM32MP151AAC Rev.Z[20...
Please tell me how to set the wake-up button (PA0:PWR_WKUP) as a return factor from LPLV-Stop mode and set STM32MP157f-EV1 to LPLV-Stop mode.
Isn't there a script file for generating RAW images for eMMC like the "create_sdcard_from_flashlayout.sh" file for generating RAW images for SD?Also, why is SD memory mapping different from eMMC memory mapping?
Kudos given to