cancel
Showing results for 
Search instead for 
Did you mean: 

Select boot mode for M4 examples not showing

JKim.2
Senior

Hello,

The starter package of STM32MP1-Ecosystem-v4.1.0 is downloaded to the SD card on STM32MP157D-EV1 board and SD booting is fine as attached log file. The tried layout files were FlashLayout_sdcard_stm32mp157d-ev1-trusted.tsv and FlashLayout_sdcard_stm32mp157d-ev1-optee.tsv

However, I don't see the below menu screen to select the boot mode for M4 examples. How can I enable the menu screen with the starter package?

Select the boot mode
1:      stm32mp157c-ev1-sdcard
2:      stm32mp157c-ev1-a7-examples-sdcard
3:      stm32mp157c-ev1-m4-examples-sdcard           <- Select stm32mp157c-ev1-m4-examples-sdcard
Enter choice: 3
3:      stm32mp157c-ev1-m4-examples-sdcard
Retrieving file: /uImage

Thanks.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0