cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.13.0 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.13.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.13.0?
    • Added the support for new microcontrollers in the STM32U5 series
    • Added the support for new microcontrollers in the STM32WBA series
    • Added the support for two new boards related to the STM32U5 series: STM32U5G9J-DK1 and STM32U5G9J-DK2
    • Added the support for one new board related to the STM32L4+ series: STEVAL-SMARTAG2
    • Added the user authentication interface to permit package download
    • Updated to Eclipse® 2023-03
    • Updated to GCC 11 support by default
    • Added CMake project support
  • Updated debug:
    • Changed values highlighted in yellow in the SFRs view
    • Debug authentication for STM32H5 products
    • Support for programming using multiple external loaders with OpenOCD
  • Updated for microprocessors:
    • Support for the latest release 5.0.0 of OpenSTLinux
    • Addition of the TCP console for semihosting output
  • Main fixed issues
    • 109036 [UC5-REGENERATE][CubeIDE][Examples]Build failed when changing some configurations of LoRaWAN_End_Node example
    • 131635 Add option to highlight when a live variable changes its value
    • 143369 STM32CubeMX Linker script generation problem
  • Known issues fixed and problems and limitations
    • Please refer to the wiki.
  • Where do I obtain STM32CubeIDE 1.13.0?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0