STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 440 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CUBE IDE debug with stm32mp157

Hello     We are using STM32CUBE ide (Ver 1.9.0) for debugging of stm32mp157a cortex-m4 core by using j-link programmer. In this, while entered into debug every time we need to select stm32mp157a cortex-m4 in j-link target settings. So, any option is...

Debugging with STM32MP135-DK

Hello,following this wiki article I'm trying to debug the sample user space application, but getting this error:It seems, I have a working serial and SSH connection to the target but the Target Status widget always shows 'Serial console in use':My De...

Screenshot 2024-03-28 112807a.png Screenshot 2024-03-28 113928.png Screenshot 2024-03-28 114311.png
ali7 by Associate II
  • 2508 Views
  • 3 replies
  • 0 kudos

stm32_programmer_cli + TSV + OTP programming

Hello,Can a line entry be added to a TSV file to flash the OTP partition?If yes, is there an example TSV file?If not, would the line below work?#Opt    Id       Name     Type      IP       Offset    BinaryP       0xF2     otp      Binary    none     ...

vpappano by Associate
  • 2281 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.15.0 released

STM32CubeIDE 1.15.0 was released today on st.com as well as an in-tool update patch. What is new in 1.15.0? Microcontroller and board lists aligned with STM32CubeMX v6.11.0 : STM32U0, STM32H7Rx/STM32H7Sx and STM32H523/STM32H533Added the support for t...

STM32CubeProgrammer v2.16.0 released

STM32CubeProgrammer v2.16.0 release informationNew features:• Added the support for the STM32U0 series– Flash memory/option byte/OTP programming via the debug and bootloader interfaces– RDP regression with password• Added the support for the STM32H7R...

STM32MP135

I would like to Design STM32MP135FA Processor based data logging and file accessing throgh Ethernet Kinldy suggest below application possible in STM32MP135 series Processor.1. Two ethernet going to use - One for SD card file acess / another one for F...

JMari.11 by Associate
  • 1812 Views
  • 1 replies
  • 0 kudos