STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP151C SPI5 clock much slower

I am trying to configure SPI5 on STM32MP151C where MPU is a master and ESP32C6 is a slave. The clock used in the device tree is HSI 64MHz. SPI driver is running with 2MHz configured and divisor in the SPI_CFG1 register is correctly set to 32. In the ...

vsaakian by Associate III
  • 1405 Views
  • 2 replies
  • 1 kudos

Issue regarding DDR3

HelloI'm using stm32mp157aaa3 processor in our custom board.And I'm working on DDR3L with arm-trusted-firmware(V2.5) ddr3 routines as my reference code and reference manual(RM0436) and Application not(AN5168).When I am hard-coding the register values...

Resolved! TF-A hangs on stm32mp157d-dk1

Hello all, As part of the evaluation of the 32MP15 series, I was trying to build the u-boot and TF-A binaries. I tried the u-boot SPL bring up and it seems to be working fine (except for failure to launch the Linux Kernel, as per your late updates). ...

Resolved! STM32MP131FAF7T how to program PMIC

I have a custom built  STM32MP131FAF7T board and can't set my VOUT2. The only line that is down is my VDD DDR Lines since I can't program my PMIC (STPMIC1DPQR) to have the VOUT2 to be 1.35 volts instead of 1.1 volts. My VCPU is at 1.2V, VDD is at  3....

T_Dodd by Associate
  • 1049 Views
  • 1 replies
  • 0 kudos

Resolved! Building kernel image and device tree

Hey, I'm following the Getting started tutorial and have some troubles at the chapter "Modify, rebuild and reload the Linux kernel":https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7...

oli1 by Associate II
  • 1633 Views
  • 2 replies
  • 1 kudos

DCMI resolution on STM32MP157c ?

I'm trying to use an ADV7280 videodecoder with DCMI and embedded linux on a board based on STM32157c-dk2. The decoder should output 720x576 picture resolution with the camera (PAL,CV) attached. However the DCMI seems to be in 'normal mode' which allo...

Ronte.1 by Associate II
  • 2395 Views
  • 7 replies
  • 0 kudos

SPI5 clock in STM32MP151

Working on setting up SPI bus and get a connection to ESP32C6 WiFi/BT module. Trying to configure SPI5 clock in device tree for STM32MP151. Have used different sources (HSI, HSE, PLL4Q), but the enable count on the SPI5_k clock is always zero. I am s...

vsaakian by Associate III
  • 4607 Views
  • 14 replies
  • 0 kudos