STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Using ST Yocto SDK with Docker for Windows

Hi,I've been trying to setup a cross compile environment using Docker for Windows, and I've run into a bit of trouble. I've setup the dockerfile so that during the build process of the image, I copy the SDK into the image and execute the .sh script.T...

TOlli by Senior
  • 4397 Views
  • 7 replies
  • 0 kudos

Moving LTDC pins on DK2 board?

Just wondering if I can edit the pinctrl.dsi file to change the pins to the Raspberry Pi header, rather than the HDMI encoder, so I can try DPI Raspberry Pi displays. In CubeMX the LTDC and most of the peripherals are locked, just wondering if it is ...

AJaro.2 by Associate II
  • 2841 Views
  • 5 replies
  • 0 kudos

Resolved! data exchange OpenAMP_TTY_echo

Hello,I am reimplementing the example application OpenAMP_TTY_echo in STM32MP157C-DK2.I want to exchange numerical data between M4 and dual A7. How can I do it ? which structure, channel or interface ?thanks in advance

IYetk by Associate III
  • 2004 Views
  • 4 replies
  • 0 kudos