STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SD card updates system

hi:I have a requirement that I need to update my nand flash or emmc system with an sd card.Currently, burning image with STM32CubeProgrammer is not suitable for batch updating.I hope you can support me

Yli.8 by Associate II
  • 1267 Views
  • 2 replies
  • 0 kudos

JTAG debug

I use jtag debugging m4 program, the following error, how should be resolvedOpen On-Chip Debugger 0.10.0+dev-01124-gbfb41e6 (2018-11-16-15:23)Licensed under GNU GPL v2For bug reports, read http://openocd.org/doc/doxygen/bugs.htmldebug_level: 1cortex_...

Yli.8 by Associate II
  • 2607 Views
  • 4 replies
  • 0 kudos

How to enable a third party 3.5" Display connected to LTDC port on STM32MP157C-EV1 board?

I need to test a 3.5" display connected to the LTDC port. How do I disable the 5.5" display that came with the STM32MP157C-EV1 board and use the 3.5" display? I see the ltdc_pins_a: ltdc-a-0{...} entry in the Linux source code device tree: ../linux-4...

Resolved! problems with installing fftw package

Hi! Have some problems with installing fftw package. I tried to install it to st-image-weston and st-example-image-xfce, but received same error when bitbake run do_rootfs. Can anybody explain this problem?Build Configuration:BB_VERSION          = "1...

VKare.1 by Associate II
  • 2085 Views
  • 1 replies
  • 0 kudos