STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

/dev/watchdog is always busy.

I am using the STM32MP15-DK2 dev board and with a modified device tree to enable some peripherals. I would like to use /dev/watchdog to reset if ever my application hangs. But whenever I try to open the device I get Error opening watchdog device: Dev...

ASuar.1 by Associate III
  • 3909 Views
  • 3 replies
  • 0 kudos

SPI chip/slave select issue STM32MP157

I have troubles in setting the polarity of the SPI chip select i/o for an external chip.I noticed In the reference manual that it should be changeable with SPI configuration register 2 (SSIOP bit 28) :Bit 28 SSIOP: SS input/output polarity0: low leve...

Ronte.1 by Associate III
  • 5682 Views
  • 5 replies
  • 0 kudos

STPMIC1 PWR_USB_SW with 5V input

Dear all,We are designing a board using STM32MP1 and STPMIC1 mostly as recommended in datasheet and application note. As we have a wide VIN range we added a discrete DC/DC with a 5V output that supply STPMIC1 VIN.We would like to use STMPIC1 PWR_USB_...

PGE by Associate III
  • 2827 Views
  • 6 replies
  • 0 kudos

Resolved! I have a problem with the predictive maintenance setup as described in UM2639 and dm00659285..". I get as far as "Edge computing setup complete". Then it completely stops. Any ideas?

The handshake sequence looked a bit odd too. [STMdemo1] (08:07:40): {"state": {"reported": {"Device_Type": "STEVAL-IPD005V1", "Features": [], "Firmware": ""}}}Update request with token "40d4c70c-ec71-4946-9f7b-b6ad2719d965" acceptedI have also tried ...

PHarl.1 by Associate
  • 2333 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP157 OTP voltage

Hi guys,I'm designing a custom board with STM32MP157C using the MB1263 board as reference.The MB1263 reference design shows the VDD_OTP pin tied to VDD, which is 3V3 for that particular board. My custom board uses VDD = 1V8 instead of 3V3. Should I t...

NCF by Associate II
  • 1532 Views
  • 1 replies
  • 0 kudos