STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP157 OTP voltage

Hi guys,I'm designing a custom board with STM32MP157C using the MB1263 board as reference.The MB1263 reference design shows the VDD_OTP pin tied to VDD, which is 3V3 for that particular board. My custom board uses VDD = 1V8 instead of 3V3. Should I t...

NCF by Associate II
  • 1526 Views
  • 1 replies
  • 0 kudos

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution Why?

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution...

Vlaty.1 by Senior
  • 1415 Views
  • 2 replies
  • 0 kudos

Resolved! change pin mux in TF-A build for i2c-bus i2c4

We would like to build the TF-A image with a different muxer settingfor i2c4. The usual setting is:i2c4_pins_a: i2c4-0 {   pins {      pinmux = <STM32_PINMUX('Z', 4, AF6)>, /* I2C4_SCL */      <STM32_PINMUX('Z', 5, AF6)>; /* I2C4_SDA */      bias-dis...

RGlie.1 by Associate II
  • 1947 Views
  • 2 replies
  • 0 kudos

Добрый день, �? решил одну проблему как подключить�?�? к stm32mp157a-dk1 по tcp

Good day, I solved one problem how to connect to stm32mp157a-dk1 over tcp. In the console, you need to write ifconfig eth0 192.168.1.5 ; net data-P ttyRPMSG0 ; net data-p8888 but I do not see data in the buffer ttyRPMSG0. in my program OpenAMP_TTY_ec...

Vlaty.1 by Senior
  • 1254 Views
  • 1 replies
  • 0 kudos

Resolved! gcc comand not found

Hello Everyone I wanted to Install Buildroot on my STM32MP157-DK2 according to this website:https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-basic-system/Unfortunately as a beginner with OpenST-Linux and Yocto I got stuck at that ste...

Can't boot from SD card on STM32MP157A-EV1

I am trying to get this board up and running again after being away from it for a while, but I've been running into problems trying to boot from the SD card. I followed the instructions from the wiki here: https://wiki.st.com/stm32mpu/wiki/STM32MP15_...

CC by Associate II
  • 3896 Views
  • 5 replies
  • 0 kudos

I have compiled the stm32mp157 disco V2.0.0.0 Distribution package for both the x11 (matchbox desktop) and the x11-xfce image, insuring that I accept the EULA. When I run both images, response times and memory image are very large compared to V1.2

I have xfce running very well in the V1.2 Yocto Distribution system on the stm32mp157c disco board. The xfce desktop is very responsive and uses about 100M of memory. The xfce desktop using the latest V2.0.0 Distribution image however is very sluggi...

STild.1 by Associate
  • 2329 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP157AAA can not boot

Hello,PLEASE GIVE SOME HELP.We made some boards based on MP157AAA and it ran good at first.BUT it can not boot anymore after someone turn off and on the power.No information comes from UART4 after turn on power switch.I change the boot-switch to '00...

0693W000004KLOFQA4.png 0693W000004KLTFQA4.png
Ssun.21 by Associate
  • 1731 Views
  • 2 replies
  • 1 kudos