STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32mp2 RT patches ,CPUFreq can't use

Due to the default removal of CPUFreq configuration in the patch file after applying RTpatch, I am unable to obtain the current CPU frequency through the following command.reference:如何更改 CPU 频率 - stm32mpuI also try lscpu and /proc/cpuinfo and so on.T...

bugman by Associate III
  • 870 Views
  • 4 replies
  • 0 kudos

Resolved! How to config DMA2D in stm32mp13 linux

Hi Dear Sir,I am using linux6.6.48 (with st patch)based on stm32mp135d,I trying to setup DMA2D but cannot find correct dts setting. and I can see the dma2d driver is supported in this kernel. but how to config dma2d in dts ?please help. thank you ver...

inman by Associate II
  • 1007 Views
  • 7 replies
  • 0 kudos

Resolved! PROBLEM: first boot STM32MP257F-EV1

I'm trying to perform the first boot on the STM32MP257F-EV1 following this guide: STM32MP25 Evaluation boards - Starter Package.  I've connected the LCD screen to the board according to the instructions.The board is powered by USB-C on CN21, and the ...

Zim by Associate II
  • 4810 Views
  • 7 replies
  • 0 kudos

Resolved! STM32MP257F-DK no output on HDMI

Hi everyone,I'm a beginner when it comes to STM32 MPU, and from the very beginning I've had an issue with the HDMI output on my STM32MP257F-DK board, which I received from my university. Naturally, I wanted to start with the Starter Package to explor...

Rayugo by Associate
  • 1912 Views
  • 2 replies
  • 0 kudos