cancel
Showing results for 
Search instead for 
Did you mean: 

soc:pin-controller-z@54004000 failed with error -22

mikel
Associate

Hello!

 

I am getting this error, and tried everything I think, getting this error:
root@br-elec-01011-mu-rvt70hsmnwc00:~# dmesg | grep error && ls -l /dev/ttySTM*
[ 1.286601] stm32mp157-pinctrl: probe of soc:pin-controller-z@54004000 failed with error -22

 

Not sure if it is ok or not. Main components seems to work fine. But I am new to this, so not sure if it can cause issues along the way.

 

 

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @mikel 

May you provide further context and information ? 

eg your Linux Device Tree. ( dtb is fine) 

Thx

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Interesting I've attached files originally but looks like I've made a mistake.
Attached the final dts and dtb files. kernel tf-a and u-boot