STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have an STM32MP157F-DK2 and am attempting to create a build using Yocto. I am using meta layers poky, openembedded, and st-stm32mp. I can build core-image-minimal. This build lacks WiFi and USB OTG which are needed.

The image that comes with the board has WiFI and USB OTG working. I am adding additional networking (VPN, firewall) to my Yocto build. I have attempted to build core-image-base and am able to see the wlan0 adapter but something in that build is disab...

KBarr.1 by Associate
  • 1083 Views
  • 0 replies
  • 0 kudos

Resolved! stm32mp157c rpmsg comminucation problem

Hello,I am working stm32mp157c. It has two processor (A7 and M4). They can communicate with each other over virt uart(rpmsg). When I want to send a message to a7 over m4, if the message is filled with constant data, everything is ok. If the message ...

aliMesut by Associate III
  • 6637 Views
  • 10 replies
  • 0 kudos