STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is it possible to load an OS on a custom board using STM32Cube tools instead of an evaluation board?

I am currently developing using STM32mp157fad and have a question. Here are the steps I have taken:Used STM32CubeProgrammer to upload the stm32mp157f-ev1 image to an SD card.Used STM32CubeMX to configure the GPIOs to be used with stm32mp157fad, gener...

KNam.2 by Associate II
  • 1679 Views
  • 1 replies
  • 0 kudos

Optee PKCS11 TA Performance really bad!

Hello, I use Optee on a stm32mp157f-dk2 board, version is the and the corresponding BSP :optee-os 3.16.0-stm32mpu-boot v2021.10-stm32mpLinux v5.15-stm32mpAll my changes are committed and built using a yocto meta-layer : https://github.com/embetrix/m...

AZaki.2 by Associate III
  • 5072 Views
  • 5 replies
  • 0 kudos

Resolved! Can ST please provide a guide for bringing up a custom board without using the STPMIC?

Can ST please provide a guide for bringing up a custom board without using the STPMIC? We are extremely space constrained and unable to fit the PMIC. For our use case we just want simple LDO's with bucks as required.There is no material I can find th...

damien1 by Associate II
  • 2066 Views
  • 2 replies
  • 0 kudos