STM32 MCUs
From FAQs to complete How-to articles, find useful articles on STM32 MCUs programming, troubleshooting, ecosystem, and product details.
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge base articles

STM32N6 FSBL explained

Summary The first stage bootloader (FSBL) is a key component in the boot process of STM32N6 microcontrollers. It is responsible for initializing the system, configuring the hardware, and loading the application code from external memory into the int...

BMontanari_0-1737488193179.png BMontanari_1-1737488193181.png BMontanari_2-1737488193184.png BMontanari_3-1737488193187.png

How to configure STM32 VS Code extension to use OpenOCD

Summary The STM32 VS Code extension doesn’t natively support OpenOCD, but with some simple configuration, you can integrate it into your debugging workflow. This article covers how to set up OpenOCD (either Streamline or ST’s fork) with the extension...

STM_Thirty2_0-1732844454636.png STM_Thirty2_1-1732844636529.png STM_Thirty2_2-1732844759012.png scrnshot.jpg

FAQ: STM32 HAL UART driver - API and callbacks

Summary This article covers the following:  How to use STM32 HAL UART driver API and Callbacks?What are the callbacks involved in UART TX / RX?How are these callbacks called?Why is the callback not called? 1. STM32 HAL UART supports 3 modes for trans...

81.png 82.png 84.png 85.png

Using VS Code for FreeRTOS™ application debugging

Introduction  In this article, we explore how to set up and debug a FreeRTOS™ project for the STM32H753 microcontroller using visual studio code (VS Code). We cover the necessary extensions, step-by-step project creation, and debugging processes, inc...

Extensions.png Tasks creation.png vTaskDelay.png Project generation.png
Sarra.S by ST Employee
  • 8741 Views
  • 0 comments
  • 0 kudos

Helpful tips on using VS Code with STM32

Summary This article highlights some tips on using VS Code with STM32. In this article, we cover the following: Performing a clean build of your project and deleting the cacheAdding source files, directories, and include files to your VS Code project...

B_Subramanian_0-1733431777905.png B_Subramanian_1-1733431777909.png cmakelists.png B_Subramanian_3-1733431777914.png

How to create a custom build setup in STM32CubeIDE

This article covers how to create a custom build setup to allow users to customize, modify, and add specific build settings for each file, folder, or project. Introduction Creating a custom build in STM32CubeIDE can be a powerful tool for developers...

BMontanari_0-1705600232962.png BMontanari_1-1705600232966.png BMontanari_2-1705600232967.png BMontanari_3-1705600232968.png

How to wake up the STM32U5 from STOP2 using LPUART

This article will show you how wake up the STM32U5 MCU from Stop 2 Low Power mode using the LPUART1 supplied by LSE or HSI Clock Source. By the end of this article, you will know the needed steps to properly set the LPUART, RCC and PWR peripheral reg...

566.jpg 567.png 569.png 571.png

Why NRST pin as GPIO mode is holding the MCU under reset

Introduction The NRST pin can be configured in GPIO mode and this is handy for small packages such as STM32C011 8-pin package. In this article, we explain the constraints and potential workaround of using NRST pin in GPIO mode. STM32C011D6Yx 8pin pa...

STea_1-1733827858859.png STea_0-1733847673174.png STea_2-1733828435310.png
STea by ST Employee
  • 4818 Views
  • 0 comments
  • 2 kudos

Troubleshooting bxCAN issues in Loop back mode on STM32 MCUs

Introduction As many know, CAN test mode is used for debug or test. One of the test modes is the CAN Loop back mode which is mainly used when only one CAN node is available, and the user needs to test the CAN functionality with no need to establish ...

SofLit_0-1733738092058.png SofLit_0-1733739357109.png
mƎALLEm by ST Employee
  • 3076 Views
  • 0 comments
  • 2 kudos

Injecting and handling ECC errors in STM32H7 flash memory

Summary This article provides practical steps showing how to inject and check single and double ECC errors in STM32H7 flash memory. Find attached to the article a ECC Flash project for testing purposes.  Introduction In the STM32H7 microcontrollers, ...

Laurids_PETERSEN_0-1730282566039.png Laurids_PETERSEN_4-1730283300046.png Laurids_PETERSEN_5-1730283318504.png Laurids_PETERSEN_6-1730283506754.png

Understanding VCONN in STM32 and TCPP USB Type-C® port protection

Introduction VCONN is a dedicated power supply pin in the USB Type-C® connector. It provides power to the cables electronics, such as e-markers (EMC), long cables with data repeaters, and VCONN-powered USB devices. It ensures proper power supply ...

FBL_0-1733410931461.png
FBL by ST Employee
  • 7883 Views
  • 0 comments
  • 1 kudos