2020-07-25 08:15 PM
Not sure if this is the best place to ask, but essentially I want to modify the LoRaWAN end-node example for STM32L476 using SX1262 transceiver to work with an STM32L433 mcu, initially making use of a Nucleo-L433RC-P board with a transceiver module wired to it, eventually shifting this to a custom board with STM32L433.
Have done something similar before for the STM32L073 processor, although that was more straightforward as that mcu is one of the example ones provided in the STM LoRaWAN code.