2024-10-16 5:50 AM - last edited on 2024-10-16 8:13 AM by mƎALLEm
Hi
I am using a STM32L433 and have a digital input pin, which is checked on bootup and enables the USB if 3.3v is in the pin. When working in debug mode, it always works, but when I switch to release mode , using stm32CubeIDE , it always reads 0v, and my optimization is None. Below is my code .
RCC->AHB2ENR |= RCC_AHB2ENR_GPIOBEN; //Enable Port B clock
GPIOB->MODER &= ~GPIO_MODER_MODE12; //PB12 as input, check for usb interaction
inSetupMode=(GPIOB->IDR >> 12 )& 1; //=1 when using USB
Can anyone let me know what the issue is?
Many thanks
Scott
Solved! Go to Solution.
2024-10-16 9:16 AM
After the write
See how HAL does the clock enables, reads back to insure writes complete first, as forces IN-ORDER-COMPLETION for the write buffers and pipeline, and adds perhaps 4 bus cycles to the transaction.
#define __HAL_RCC_GPIOB_CLK_ENABLE() do { \
__IO uint32_t tmpreg; \
SET_BIT(RCC->IOPENR, RCC_IOPENR_GPIOBEN); \
/* Delay after an RCC peripheral clock enabling */ \
tmpreg = READ_BIT(RCC->IOPENR, RCC_IOPENR_GPIOBEN); \
UNUSED(tmpreg); \
} while(0U)
2024-10-16 6:07 AM
Hard to know.
Enable the clocks early. There is a hazard enabling the clock and then immediately writing the peripheral registers.
Read back the RCC->AHB2ENR / _DSB()
2024-10-16 7:01 AM
Hi ,
what is _DSB?
What do I check ? Is it if the B clock is enabled?
And if its not what do I do if its not enabled?
Sorry for all the questions.
Scott
2024-10-16 7:08 AM
Not a check, just small delay. Also, I would suggest adding some small delay between MODER setting and reading the IDR.
2024-10-16 7:10 AM
Potential with all clocks, whilst design is synchronous, probably a couple of gates deep, to reset and start properly.
DSB is a fencing instruction, clearing the pending write buffers
https://www.eevblog.com/forum/programming/stm32-__dsb()-vs-reading-back-register/
The HAL has a lot of lag and function calls, where as optimized register level code will potentially get you back-to-back pipelined writes, hence the hazard.
See how the HAL reads back the RCC register, this forces the pending writes to complete.
2024-10-16 7:22 AM
Many thanks for the reply. I will add a delay.
Thanks
Scott
2024-10-16 7:24 AM
Many thanks for your reply.
I havent come across this before, do I call it for all clocks, or is it 1 command takes care of it all?
I can add "__DSB();" line to my code, is that all is needed?
Regards
Scott
2024-10-16 8:11 AM
I added the line:
__DSB();
after the clocks being enabled, but never made a difference.
But when I added a 2ms delay after GPIOB->MODE and this worked.
Where do I add the DSB command, and is it just the DSB() on its own?
CHeers
Scott
2024-10-16 9:16 AM
After the write
See how HAL does the clock enables, reads back to insure writes complete first, as forces IN-ORDER-COMPLETION for the write buffers and pipeline, and adds perhaps 4 bus cycles to the transaction.
#define __HAL_RCC_GPIOB_CLK_ENABLE() do { \
__IO uint32_t tmpreg; \
SET_BIT(RCC->IOPENR, RCC_IOPENR_GPIOBEN); \
/* Delay after an RCC peripheral clock enabling */ \
tmpreg = READ_BIT(RCC->IOPENR, RCC_IOPENR_GPIOBEN); \
UNUSED(tmpreg); \
} while(0U)