2022-06-28 08:23 AM
I have two P-Nucleo-WB boards and both of them end up in this state.
CubeIDE trying to load binary:
CubeProgrammer:
Found several topic that looks the same however nothing helped. Has anyone solved this problem?
2022-06-28 11:41 AM
Configure connect mode to Under reset
2022-06-28 12:47 PM
I have tried to connect it "Under reset mode" with pressed reset button. Result is the same:
2022-06-29 07:04 AM
Seems power on your board is unstable. Check it ... Under reset is mode not presed but
2022-07-01 12:30 AM
Power comes from USB port and it's the same on other ports. Connecting under reset results in this same error. Is there any other method I could try to bring back my stm?
2022-07-01 03:49 AM
I have managed to run board in bootloader mode and successfully connect with CubeProgrammer through UART. I was able to load bin file. Unfortunately ST-link still does not work and I receive all the time this same error: "No device found". Any thoughts what else I can do?
2022-07-08 01:35 AM
Hello,
Your power supply seems to be very low, maybe you can try to change your usb cable.
Best Regards
2022-07-08 02:56 AM
I have checked voltage on my both boards and it seems like both of them got this same issue with voltage:
First board:
5V pin measured 2.5 V and 3V3 pin measured 2.3 V
Second board:
5V pin measured 5 V and 3V3 pin measured ~0 V
Strange is that I have taken precautions after first board failed and only think I did with board was plug/unplug st-link usb cable.
2022-07-08 05:53 AM
Hello,
In order to use ST LINK port, ensure that JP1 is on USB STL position.
Best Regards
2022-07-18 04:31 AM
Hi Remy,
Jumpers are ok. I had right voltage before. It seems like I have bricked somehow two this same boards with my program. With first I had doubts if I have break it with some static charge but with second I was rather cautious doing stuff and yet, it still got broken. Do you think it is recoverable?
Best regards