cancel
Showing results for 
Search instead for 
Did you mean: 

Cant upload to NUCLEO-F411RE if I have a HC-06 Bluetooth module attached

NicRoberts
Senior II

When I have the HC-06 powered from the board (either 3.3V or 5V) & try to upload to the board I get,

 

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target.

 

Yet when I unhook the module from the board everything uploads fine.

So, I uploaded to check my debug serial connection without the HC-06 connected, all fine.

Hook up the module, no debug . Its as if connecting it up to the power on the board knocks out the USB-ST-Link.

 

When I plug into the 5V - debug drops, LED3 goes out & LED1 starts flashing.

When I plug into to 3.3V - debug stops but the LEDs remain on.

I've swapped out the HC-06 module but I still get the same behaviour,

 

All power is being supplied by the US-ST-Link

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
NicRoberts
Senior II

Turns out I'm an *** & had shorted the 5v & GND by putting the module in the breadboard at the wrong orientation.

 

 

View solution in original post

3 REPLIES 3
Pavel A.
Super User

So... have the HC06 powered from something else? The USB supply via the Nucleo connector is limited.

 

 

Andrew Neil
Super User

What "HC-06 module", exactly?

Show your schematic of how you have this BT module connected.

Have you checked the supply voltage when it is connected?

The ST-Link should report the voltage it is seeing...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
NicRoberts
Senior II

Turns out I'm an *** & had shorted the 5v & GND by putting the module in the breadboard at the wrong orientation.