I have two P-Nucleo-WB boards and both of them end up in this state.CubeIDE trying to load binary:CubeProgrammer: Found several topic that looks the same however nothing helped. Has anyone solved this problem?
Hi All,Thanks for all your replies. I have tested voltages with few chargers and still got this same result.Tested both ports: USB MCU and ST-LINK (jumpers in correct settings). I am not using any USB hub. I used to plug it directly to laptop - lapto...
Hi Remy,Jumpers are ok. I had right voltage before. It seems like I have bricked somehow two this same boards with my program. With first I had doubts if I have break it with some static charge but with second I was rather cautious doing stuff and ye...
I have checked voltage on my both boards and it seems like both of them got this same issue with voltage:First board:5V pin measured 2.5 V and 3V3 pin measured 2.3 VSecond board:5V pin measured 5 V and 3V3 pin measured ~0 VStrange is that I have take...