cancel
Showing results for 
Search instead for 
Did you mean: 

What is the soldering profile for the STM32WB35CCU6A MCU?

VVakh.1
Associate III

The operating temperature range for the above MCU is -40 to 85 deg C (105 deg C junction). Does it mean that the maximum temperature for soldering is 105 deg C, or does it just mean that the MCU will shut down at 105 deg C? I would appreciate it if you refer to any official application note.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

85C (105C junction) is the max operating temperature. Junction temperature is what actually matters here. Beyond that range the behavior is no longer guaranteed.

Soldering will need to be quite a bit hotter.

https://www.st.com/resource/en/application_note/an2639-soldering-recommendations-and-package-information-for-leadfree-ecopack-mcus-and-mpus-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

85C (105C junction) is the max operating temperature. Junction temperature is what actually matters here. Beyond that range the behavior is no longer guaranteed.

Soldering will need to be quite a bit hotter.

https://www.st.com/resource/en/application_note/an2639-soldering-recommendations-and-package-information-for-leadfree-ecopack-mcus-and-mpus-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".
VVakh.1
Associate III

Thank you