2025-03-14 3:18 AM - edited 2025-03-14 3:25 AM
Hello,
i' m using STM32CubeIDE with Nucleo-WB05KZ .
i started with the exemple of BLE_p2pServer, so i imported the project and when i tried to Run the project i get this error : Program "make" not found in PATH
there an extention "make" to install also ?
thanks
2025-03-14 8:42 AM
Hello @ljm
Please use the example available on the last version of the STM32CubeWB0 (download the STM32CubeWB0 from our ST Website and not from GitHub) and make sure to use the STM32CubeIDE V1.18.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.