2025-04-01 5:10 AM - edited 2025-04-01 5:12 AM
So I'd been merrily using STM32CubeIDE all morning, doing the usual code-download-debug cycle with no problems at all.
Then, after some code updates & successful build, it suddenly can't reach the GDB server:
STMicroelectronics ST-LINK GDB server. Version 7.4.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Failed to bind to port 61234, error code -1: No error
Failure starting GDB server: TCP port 61234 not available.
Shutting down...
Exit.
Several people seem to have had this recently; eg,
So why should this change when nothing has been updated - I'm just working in the IDE as usual ?!
This is CubeIDE v1.13.0 - so old, yes - but surely no reason for it to just give up in the middle of a session?
On Windows-11 - no updates have happened.
Solved! Go to Solution.
2025-08-04 3:09 AM
@Andrew Neil wrote:Restarting the IDE made no difference.
Restarting the PC restored operation.
Would still like to know why the sudden failure to bind to the port ?
Maybe this explains it:
In another thread, @STackPointer64 wrote:Restarting the computer will also resolve the issue, as it terminates the hanging process during shutdown. However, simply restarting the IDE won’t help because the GDB server runs as a separate process.
While the IDE normally starts and stops this process, it sometimes fails to terminate it when it hangs.
(my emphasis)
2025-04-01 9:29 AM
Restarting the IDE made no difference.
Restarting the PC restored operation.
Would still like to know why the sudden failure to bind to the port ?
2025-04-01 2:36 PM - edited 2025-04-01 2:52 PM
The same old question: is any antivirus (or VPN, or corporate brain-***ing-ware) installed?
AFAIK these ports are not reserved in Windows in any way. So other apps or Windows components can steal them.
Update: The helpful AI informs that user can define several ranges of ports to exclude from automatic allocation - but this won't prevent other apps to use these ports explicitly. The command is netsh int ipv4 add excludedportrange protocol=tcp startport=<port_number> numberofports=<N>
2025-04-01 4:22 PM - edited 2025-04-01 4:24 PM
@Pavel A. wrote:The same old question: is any antivirus (or VPN, or corporate brain-***ing-ware) installed?
Just the standard Windows Defender.
But why would it suddenly start blocking this port - and stop blocking it after a reset?
The firewall exceptions are already set up - otherwise it wouldn't have been working for all these years.
@Pavel A. wrote:So other apps or Windows components can steal them.
Again, what would suddenly steal it - and stop after a reset?
Why has it not happened before?
What can be done to see if it's a problem with GDB itself, or with some thing(s) else "blocking" or "stealing" GDB's port?
2025-04-01 7:23 PM
Have you tried to change the port - after checking the active busy and reserved ports, disable Windows firewall?
To check busy ports: netstat -ano
To check reserved ports: netsh int ipv4 show excludedportrange tcp active , netsh int ipv4 show excludedportrange udp active
2025-04-02 12:45 AM
@Pavel A. wrote:Have you tried to change the port
Here?
@Pavel A. wrote:after checking the active busy and reserved ports
Microsoft Windows [Version 10.0.26100.3476]
(c) Microsoft Corporation. All rights reserved.
>netstat -ano
Active Connections
Proto Local Address Foreign Address State PID
:
TCP 0.0.0.0:61234 0.0.0.0:0 LISTENING 356
TCP 0.0.0.0:61235 0.0.0.0:0 LISTENING 356
:
TCP 127.0.0.1:60275 127.0.0.1:61234 ESTABLISHED 12276
TCP 127.0.0.1:60277 127.0.0.1:61234 ESTABLISHED 4548
TCP 127.0.0.1:61234 127.0.0.1:60275 ESTABLISHED 356
TCP 127.0.0.1:61234 127.0.0.1:60277 ESTABLISHED 356
:
>netsh int ipv4 show excludedportrange tcp active
Protocol tcp Port Exclusion Ranges
Start Port End Port
---------- --------
49692 49791
49892 49991
50000 50059 *
50060 50159
50160 50259
50260 50359
61893 61992
63720 63819
* - Administered port exclusions.
>netsh int ipv4 show excludedportrange udp active
Protocol udp Port Exclusion Ranges
Start Port End Port
---------- --------
50000 50059 *
63654 63753
63854 63953
63954 64053
64054 64153
64154 64253
64694 64793
65015 65114
* - Administered port exclusions.
>
But, again, it's all back to working now - and had been for several years. Why would it just change?
I shall have to try to remember this thread if it happens again ...
2025-06-25 5:02 AM
@Andrew Neil wrote:Restarting the PC restored operation.
Also here:
@Andrew Neil wrote:Would still like to know why the sudden failure to bind to the port ?
Remains a mystery!
2025-06-25 10:17 AM - edited 2025-06-25 10:23 AM
This can be effect of some "endpoint protection" software such as some versions of manageengine.com.
Likely will be fixed soon or already fixed. This **** is managed remotely so it can change its behavior without user knowing it.
2025-08-04 2:54 AM
@Andrew Neil wrote:
@Andrew Neil wrote:Would still like to know why the sudden failure to bind to the port ?
Remains a mystery!
If it happens again, I'll try to remember to give this a go - from @STackPointer64
2025-08-04 3:09 AM
@Andrew Neil wrote:Restarting the IDE made no difference.
Restarting the PC restored operation.
Would still like to know why the sudden failure to bind to the port ?
Maybe this explains it:
In another thread, @STackPointer64 wrote:Restarting the computer will also resolve the issue, as it terminates the hanging process during shutdown. However, simply restarting the IDE won’t help because the GDB server runs as a separate process.
While the IDE normally starts and stops this process, it sometimes fails to terminate it when it hangs.
(my emphasis)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.