cancel
Showing results for 
Search instead for 
Did you mean: 

LoRaWAN Middleware to SubGHz_Phy middleware connectivity

pho3nix
Associate III

!!Naive question!!

I have started LoRa development recently, I am using RAK3172 module which has STM32WLE5CCU6 embedded with it. Now during the development, I am seeing that the module is transmitting and joining the server but it is not getting any join confirm status. So, after going through AN5406 I came through the MSC of Class A Tx-Rx. I am having some issues to understand the message flow of this part,

dynamic msc.png

static msc.png

which functions are responsible for communication of LoRaMac.c file with Radio.c, as there is no RadioSend function is present in the LoRaMac.c file according to the application note.

Any help would be appreciated, thank you.

0 REPLIES 0