STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WB55 beacon

Using STM32WB55 as iBeacon, and Low Power mode (STOP2), the firmware on function MX_APPE_Process();doesn't return to my firmware, so how can I change contents of advertising data ?I tried a timer to have my firmware run, it does, but it seems to me t...

rbenv.3 by Associate II
  • 1646 Views
  • 1 replies
  • 1 kudos

Resolved! How to use BLE_p2pServer example with NUCLEO-WBA52CG board?

Hi,I would like to use the BLE_p2pServer example with the NUCLEO-WBA52CG board as shown in the MOOC example with the NUCLEO-WBA55CC board. Unfortunately, I can only find this example for the NUCLEO-WBA55CG via the “Example Selector”.Is there a way to...

ledi7 by Associate III
  • 1572 Views
  • 1 replies
  • 0 kudos

Resolved! Quad SPI Single Mode Read Chip ID from Riverdi

Hello,I'm using a Nucleo-WB55RE board with Quad SPI in single mode.  I'm trying to start very simply by just reading the chip id from a Riverdi BT81X display.  I have captured two waveforms, one via a Nucleo-446 board using regular SPI and one from t...

kumaichi_0-1725599716789.png kumaichi_1-1725600004560.png

I am using a NUCLEO-WL55JC1 and the LoRaWAN_End_Node example. I want to add USART1 to the example, so that I can forward the UART data over LoRa. The problem is that the interrupts for USART1 never trigger if the LoRaWAN process is also running.

If I comment out "MX_LoRaWAN_Process();" in main, then the USART1 interrupts trigger as they normally would. Could anyone offer some advice of how to add USART1 to the example?Kind regards

BBI Louw by Associate
  • 1523 Views
  • 1 replies
  • 2 kudos

Resolved! USBX Dual Composite CDC ACM not working

Hello all,   I am trying to add two virtual COM ports on STM32WB5MMHGx device. The initial code is based out of STM32Cube example: Ux_Device_CDC_ACM. I initially added this piece of code to register the class.       cdc_acm_parameter2.ux_slave_clas...

NRedd.2 by Senior
  • 3370 Views
  • 3 replies
  • 1 kudos