Skip to main content
Senior II
November 26, 2024
Solved

Can the USBPD software be used without the TCPP hardware?

  • November 26, 2024
  • 1 reply
  • 755 views

I need to have USB PD connectivity so I am using the examples provided. There are SNK and SRC and DRP examples. However, they all use the TCPP which is also included in all of the 3 demo boards. I don't see any way to disable the TCPP component itself and keep using the X-CUBE-TCPP middleware because it seems there is a library file provided that has the TCPP manipulation within it and I can't edit that file.

Is there any recommended strategy for developing a USBPD application on the STM32G071 that does not include the use of the TCPP hardware? I can uncheck the Board Part and the Board Support package but then I don't get good code generation.

 

Thanks

This topic has been closed for replies.
Best answer by FBL

Hi @Carl_G 

Sure, USB PD can be used without the TCPP hardware.

X-CUBE-TCPP is dedicated package. For that reason, it cannot be customized.

1 reply

FBLBest answer
ST Technical Moderator
December 3, 2024

Hi @Carl_G 

Sure, USB PD can be used without the TCPP hardware.

X-CUBE-TCPP is dedicated package. For that reason, it cannot be customized.
To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL