2022-02-27 12:02 AM
2022-02-28 12:48 AM
There's only one radio - so it can only be doing one thing at any one time.
You would have to devise some sort of time-sharing scheme...
2022-02-28 2:15 AM
It seems that SiLabs own the Z-Wave IP, and the only 3rd-party licensee is Mitsumi - so no STM32 support at all?
2022-02-28 3:51 AM
2022-03-01 2:46 AM
I haven't looked into how they do it, but I don't see any particular reason to assume that it must be (custom) hardware?
2022-03-02 12:49 AM
Hello,
There is no support on STM32WL for LoRa and Zwave concurrency. We haven't any exemple, so it's up to you to create your application.
regards
2022-03-02 2:00 AM
@Louis AUDOLY - Does ST have any support at all for Zwave ?
2022-03-02 2:03 AM
Hello,
No sorry we don't have any support on this protocol.
Regards
2022-03-02 2:20 AM
This application note describes who the "concurrency" is managed:
So it does, indeed, use specific hardware. But note that the WB chip has specific IEEE 802.15.4 and BLE hardware - which is not the case for LoRa / Zwave in the WL.
See recent post from @Louis AUDOLY confirming that ST have no support at all for Zwave.