cancel
Showing results for 
Search instead for 
Did you mean: 

I Nucleo lrwan problem

Hamdi Oussema
Associate II

I'm currently using I Nucleo lrwan1 shield and STM32L073 to create a Lora end node. I downloaded the latest I cube lrwan (v2.0.0) and there is no configuration to the I Nucleo lrwan1. So I can't make it work.

So, is there anyone who has the same problem or can anyone guide me to make it work.

I also posted the problem on the TTN forum and they recommended me to ask the st community about this problem

here is the link : https://www.thethingsnetwork.org/forum/t/i-cube-lrwan-problem/48864/3

23 REPLIES 23

Thanks, I'll try to find a solution and Ill post it here

@Community member​ : "Not sure ST provides firmware for the USI model"

They don't provide firmware for the USI module itself, but they do provide the AT_Master project to communicate with the USI module when it's mounted on a Nucleo board.

Unfortunately, they appear to have broken it in I-CUBE-LRWAN v2.0.0 (March 2021) :

https://community.st.com/s/question/0D53W00000vP1XtSAK/icubelrwan-v200-with-nucleol073rz-board-and-inucleolrwan1-shield

@Imen DAHMEN​ - any chance of getting anyone at ST to look into this?

PS

@Imen DAHMEN​ - or, at least, provide a download link for v1.3.1 in the meantime ...

Imen.D
ST Employee

Hello,

I will try to contact expert internally to review this post.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

https://drive.google.com/file/d/1Y141OfbyeC7fU71ZG7caRJ_xn7j1oe25/view?usp=sharing

The older versions used to present, I do have this stuff archived

There were some other reports of the support of the USI being an issue, and generally that LRWAN2 and LRWAN3 could do with some actual ownership/responsibility rather than being delivered pre-abandoned..

On another front I did port V1.1.1 to an STM32F103 platform, ~900 MHz LoRaP2P with supposedly a 2W PA driven via an 8-bit I2C DAC, toasty..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for the Zip.

"There were some other reports of the support of the USI being an issue"

Indeed - my name would be on some of them. It took ages to get them just to publish the schematics of the I-NUCLEO-LRWAN1 board.

:\

"and generally that LRWAN2 and LRWAN3 could do with some actual ownership/responsibility rather than being delivered pre-abandoned.."

Likewise.

ST tout these as "Partner" companies & products - there really needs to be some better commitment from both ST and these "Partners" to provide and maintain a decent level of documentation.

Perhaps @Imen DAHMEN​  could also find someone to look into that ... ?

thanks - ST expert has responded in this thread:

https://community.st.com/s/question/0D53W00000vP1XtSAK/icubelrwan-v200-with-nucleol073rz-board-and-inucleolrwan1-shield

It is confirmed that the AT_Master project in I-CUBE-LRWAN v2.0.0 (March 2021) does not work out-of-the-box.

Imen.D
ST Employee

You are welcome.

Thank you for your contribution and thank you for your patience while we work on this.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Andrew Neil
Evangelist III

@Community member​ "there is no configuration to the I Nucleo lrwan1"

Not quite sure what you mean by that?

Hamdi Oussema
Associate II

@Andrew Neil​ as you can see here : https://github.com/USIWP1Module/USI_I-NUCLEO-LRWAN1 there are some configurations to be done depending on the I cube lrwan version.

Hmm ... I thought I'd replied to that yesterday?

That page refers to a very old version of I-CUBE-LRWAN - I just followed the instructions in the P-NUCLEO-LRWAN2 User Manual.

But it has been noted that these need updating for v2.0.0 of the I-CUBE-LRWAN:

https://community.st.com/s/question/0D53W00000wVhzTSAS/icubelrwan-the-things-stack-v3-replaces-the-things-network-v2

>:(