cancel
Showing results for 
Search instead for 
Did you mean: 

I-CUBE-LRWAN v2.0.0 with B-L072Z-LRWAN1 ?

Andrew Neil
Super User

Can anyone either confirm or deny that the End_Node project from I-CUBE-LRWAN v2.0.0 works with the B-L072Z-LRWAN1 (with Murata Type-ABZ module) ?

https://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html

And any tutorials on getting it talking with The Things Network (TTN) ?

(tutorials I've seen previously were for v1.3.1 - and v2.0.0 looks rather different).

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Andrew Neil
Super User

Well, not a good start: building straight "out-of-the-box" - 57 Warnings:

0693W00000BcvXIQAZ.png 

Which would seem to summarise as 3 real issues, repeated:

0693W00000BcvfzQAB.png 

ADDENDUM

Sure enough, the REGION_EU868 and X_NUCLEO_IKS01A2 options are defined both in the Project setting and in source files:

0693W00000BcvuGQAR.png

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

The warning that 'fBuffer' may be used uninitialized seems to be from GCC inlining 'static' functions - as the warning is reported in PrepareFrame(), but the definition of fBuffer is in LoRaMacMcpsRequest()

PrepareFrame() is called by Send() which is called from LoRaMacMcpsRequest():

LoRaMacStatus_t LoRaMacMcpsRequest( McpsReq_t* mcpsRequest, bool allowDelayedTx )
{
    GetPhyParams_t getPhy;
    PhyParam_t phyParam;
    LoRaMacStatus_t status = LORAMAC_STATUS_SERVICE_UNKNOWN;
    LoRaMacHeader_t macHdr;
    VerifyParams_t verify;
    uint8_t fPort = 0;
    void* fBuffer;                           // <=== *** Defined here
    uint16_t fBufferSize;
    int8_t datarate = DR_0;
    bool readyToSend = false;
 
    if( mcpsRequest == NULL )
    {
        return LORAMAC_STATUS_PARAMETER_INVALID;
    }
    if( LoRaMacIsBusy( ) == true )
    {
        return LORAMAC_STATUS_BUSY;
    }
 
    macHdr.Value = 0;
    memset1( ( uint8_t* ) &MacCtx.McpsConfirm, 0, sizeof( MacCtx.McpsConfirm ) );
    MacCtx.McpsConfirm.Status = LORAMAC_EVENT_INFO_STATUS_ERROR;
 
    // AckTimeoutRetriesCounter must be reset every time a new request (unconfirmed or confirmed) is performed.
    MacCtx.AckTimeoutRetriesCounter = 1;
 
    switch( mcpsRequest->Type )
    {
        case MCPS_UNCONFIRMED:
        {
            readyToSend = true;
            MacCtx.AckTimeoutRetries = 1;
 
            macHdr.Bits.MType = FRAME_TYPE_DATA_UNCONFIRMED_UP;
            fPort = mcpsRequest->Req.Unconfirmed.fPort;
            fBuffer = mcpsRequest->Req.Unconfirmed.fBuffer;
            fBufferSize = mcpsRequest->Req.Unconfirmed.fBufferSize;
            datarate = mcpsRequest->Req.Unconfirmed.Datarate;
            break;
        }
        case MCPS_CONFIRMED:
        {
            readyToSend = true;
            MacCtx.AckTimeoutRetries = MIN( mcpsRequest->Req.Confirmed.NbTrials, MAX_ACK_RETRIES );
 
            macHdr.Bits.MType = FRAME_TYPE_DATA_CONFIRMED_UP;
            fPort = mcpsRequest->Req.Confirmed.fPort;
            fBuffer = mcpsRequest->Req.Confirmed.fBuffer;
            fBufferSize = mcpsRequest->Req.Confirmed.fBufferSize;
            datarate = mcpsRequest->Req.Confirmed.Datarate;
            break;
        }
        case MCPS_PROPRIETARY:
        {
            readyToSend = true;
            MacCtx.AckTimeoutRetries = 1;
 
            macHdr.Bits.MType = FRAME_TYPE_PROPRIETARY;
            fBuffer = mcpsRequest->Req.Proprietary.fBuffer;
            fBufferSize = mcpsRequest->Req.Proprietary.fBufferSize;
            datarate = mcpsRequest->Req.Proprietary.Datarate;
            break;
        }
        default:           // <=== *** this potentially leaves fBuffer uninitialised
            break;
    }
 
    // Get the minimum possible datarate
    getPhy.Attribute = PHY_MIN_TX_DR;
    getPhy.UplinkDwellTime = MacCtx.NvmCtx->MacParams.UplinkDwellTime;
    phyParam = RegionGetPhyParam( MacCtx.NvmCtx->Region, &getPhy );
    // Apply the minimum possible datarate.
    // Some regions have limitations for the minimum datarate.
    datarate = MAX( datarate, ( int8_t )phyParam.Value );
 
    if( readyToSend == true )
    {
        if( MacCtx.NvmCtx->AdrCtrlOn == false )
        {
            verify.DatarateParams.Datarate = datarate;
            verify.DatarateParams.UplinkDwellTime = MacCtx.NvmCtx->MacParams.UplinkDwellTime;
 
            if( RegionVerify( MacCtx.NvmCtx->Region, &verify, PHY_TX_DR ) == true )
            {
                MacCtx.NvmCtx->MacParams.ChannelsDatarate = verify.DatarateParams.Datarate;
            }
            else
            {
                return LORAMAC_STATUS_PARAMETER_INVALID;
            }
        }
 
        status = Send( &macHdr, fPort, fBuffer, fBufferSize, allowDelayedTx );     // <=== *** used here

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

"Can anyone either confirm or deny that the End_Node project from I-CUBE-LRWAN v2.0.0 works"

currently unproven - due to lack of support on how to get it to work with the new TTN v3 ("The Things Stack")

It does seem to communicate with the gateway, but then the routing in TTN doesn't work.

https://community.st.com/s/question/0D53W00000wVhzTSAS/icubelrwan-the-things-stack-v3-replaces-the-things-network-v2

However, it is proven that the AT_Master project for I-NUCLEO-LRWAN1 + NUCLEO-L073RZ from I-CUBE-LRWAN v2.0.0 does not work:

https://community.st.com/s/question/0D53W00000uXu3ASAS/i-nucleo-lrwan-problem

https://community.st.com/s/question/0D53W00000vP1XtSAK/icubelrwan-v200-with-nucleol073rz-board-and-inucleolrwan1-shield

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.