2022-11-18 5:45 AM
Hello,
I made my custom board with a STM32WLE5CC micro and I am trying to program it using the SW interface. I have a ST-LINK/V2 where I connect the SWDIO, SWCLK, TRACE_SWO, NRST, VCC and GND pins from my board.
When I try to program it using STM32CubeIDE, an error jumps when the programing is at 92% (almost completed) . This is the error:
When I try to connect to the device using STM32CubeProgrammer two things happen. First thing is what we can see in the following picture:
When I try to connect in Normal mode an error jumps saying: "Cannot connect to access port. If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode" (which is weird because I never programmed this chip before, never touched the TrustZone)
So, then I try to connect in HotPlug mode and works:
However I still cannot debug my program trough STMCubeIDE because the first error persists. Besides, I guess that I should be able to connect using the normal mode.
Any help is appreciated, I am a bit lost here.
Thanks,
Asier
Solved! Go to Solution.
2022-11-21 1:46 AM
Thanks a lot for the support @MM..1. I finally found the problem and it was hardware. The reset line was connected to ground by mistake (there was an erroneous switch that made this connection). Once I unsoldered this component from the board, the programing/debugging started to work as usual!
2022-11-18 6:07 AM
You config CubeIDE debug wth some error. try show screen or check it.
2022-11-18 6:23 AM
I created a new project specific for my micro and used the default debug configuration:
I also tried enabling and disabling the SWV (Serial Wire Viewer), but the result is exactly the same. I also tried using OpenOCD, but many more errors jump...
2022-11-18 6:59 AM
2022-11-18 7:13 AM
@MM..1 Thanks for the reply. I followed the steps in the document, but I am getting the same behavior
2022-11-18 7:15 AM
Realy you set connection under reset and enable low power mode debug ?
2022-11-21 1:46 AM
Thanks a lot for the support @MM..1. I finally found the problem and it was hardware. The reset line was connected to ground by mistake (there was an erroneous switch that made this connection). Once I unsoldered this component from the board, the programing/debugging started to work as usual!