Skip to main content
Southbranch
Senior
Mar 11, 2025 1:47 PM UTC
Solved

STM32N6 with built in flash?

Hi,

Does anyone know if there is a chance for a new N6-device later this year having built in flash of at least 4MB?

Our project is currently based on a one chip solution with a custom U5-board with built in FLASH/RAM of 4MB and a 5” Riverdi display. However, we need to migrate to a 7” Riverdi display and a MCU with higher performance. We are in strong favour of shorten time-to-market by keeping a low complexity integration (i.e. no external memories) and a straightforward PCB design.

It would be really helpful to us if any plausible market intentions from ST are given.

Thanks in advance

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 11, 2025 2:03 PM UTC

Hello,

STM32N6 product is intended to be Flashless. I don't think there will be a version with an embedded flash at least in the near future (1 year).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 11, 2025 2:03 PM UTC

Hello,

STM32N6 product is intended to be Flashless. I don't think there will be a version with an embedded flash at least in the near future (1 year).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Southbranch
Senior
Mar 12, 2025 3:47 PM UTC

Thanks for your reply.

However that was disappointing to hear.

From a business point of view, I think such a product could be disruptive and offer an interesting market opportunity for ST.