cancel
Showing results for 
Search instead for 
Did you mean: 

URGENT*** PLEASE HELP**** FatFS.h no such file or directory when running from touchgfx designer, the files are included because they are generated with CUBEMX and the code complies without errors in CUBE IDE, STM32F746 Disco

BO Re.1
Associate II

when i try and flash the board through the designer it keeps failing. I have tried removing the files and creating a new folder and linking that one but no success, i am desperate my project is due to be presented on Friday, i have experimented with all parts separately and now i am combining the code, the last piece if the FatFS SDMMC, data logging, the code works perfectly as it is tried and tested, i simply dont understand why this is happening, it should be a simple process just to add code that has already worked on the 746 Disco board, although that was without the screen, but this part of the project is just data logging and has no interaction with the screen apart from sharing a task in main.c. the header is there as CubeIDE complies can someone please get back to me ASAP, it is important. here is the log from TouchGFX designer

Image is not available

Image is not available

0693W000000V7nMQAS.jpg0693W000000V7lBQAS.jpg

 0693W000000V7nMQAS.jpg

13 REPLIES 13

thanks Martin, still wont work

is there any chance you could send me a screen shot of how to fixed it, i have tried so many different variations of the include path but it doesn't work, im under a bit of pressure its for a college project that due Friday ,and im not a software developer so im not familiar with makefiles,

I presume the picture below shows the path, i have put it in, numerous times saved the file and 'Run Target', same error

0693W000000VBReQAO.jpg

This slipped my mind - How did you do on this?

I didn't get it working, the project was due , but because of the current Covid-19 ,lockdown it was submitted via video demonstrations, online presentations and video talk through of the code etc.

im in the middle of exams now but hopefully in the next few weeks ill get back to it , i would like to get working as it should ill let you how it goes and thanks for getting back to me.

regards

Barry

Allright, please let me know! 🙂