2023-07-05 1:52 AM
Hello,
I checked but I didn't find any information, is there a TouchGFX roadmap available somewhere ?
Regard,
NME
Solved! Go to Solution.
2023-07-05 8:17 AM
Hello @nme ,
You can check the changelog if you need to know what is new and what is deprecated between versions of TouchGFX. But concerning the roadmap, it's quite confidential I'm afraid. But you're more than welcomed to ask for features, we'll discuss about them internally and consider or not to develop them.
Hope that answers your question :)
2023-07-05 4:40 AM
Welcome @nme, to the community!
What exactly do you mean by roadmap?
TouchGFX is constantly being developed further, e.g. vector graphics (SVG) have also been supported for a while. What function are you looking for specifically?
Regards
/Peter
2023-07-05 5:25 AM - edited 2023-07-05 5:26 AM
Hello Peter,
I use TouchGFX on a project release 4.16.1 and as we start a new project I start to use 4.22. There's a lot of new features especially L8 compression and stock.
But for example I wanna use a vertical swipe container which is not yet available. My concern was should I develop a container or will this be included in a next release, it's not an urgent need so if it will be in a next release I will not spend time on the feature.
Nicolas
2023-07-05 8:17 AM
Hello @nme ,
You can check the changelog if you need to know what is new and what is deprecated between versions of TouchGFX. But concerning the roadmap, it's quite confidential I'm afraid. But you're more than welcomed to ask for features, we'll discuss about them internally and consider or not to develop them.
Hope that answers your question :)
2023-07-05 8:42 AM - edited 2023-07-05 8:43 AM
Hello Osman,
It answered my question even if it's not what I expected :face_savoring_food: but I understand your point of view.
Is there a specific forum to ask for features ?
Thanks,
Nicolas
2023-07-06 2:04 AM
Hi @nme ,
You're in the right place to ask for a feature ;)
2023-07-06 5:37 AM
Hi @Osman SOYKURT,
wasn't there a specian feature request forum? I remember a post where someone asked for a "collapse all" function for the left text list in the TouchGFX Designer and I can't find it anymore. As I now have about 650 texts in 25 groups a collapse all button (or just start with collapsed groups) would be great :)
2023-07-10 1:54 AM
Hello @t.decker ,
We will have a dedicated space for that in the community and you'll be able to use the "Request feature" button in TouchGFX Designer (which redirects you to an invalid link for the moment). But for the moment, you can ask features in the forum.