2021-12-29 12:36 AM
Dear Friends ,
I have an custom board that using STM32F746 + QSPI Flash (For LCD Data) + RAM (LCD Buffer) + USB Host FS + SD Card
Development tools :
CubeIDE Ver. 1.6.1
TouchGFX Ver 4.17
And using Free RTOS
I want to use SD Card and USB Host for data storage (FATFS) , when I expand LCD pages by TouchGFX I meet problem with mounting the SD card !
By removing some page or light pages the SD card working without problem
The error that I see on mounting is FR_NO_FILESYSTEM !
Also I check when I remove USB host from FAT system the SD card works without problem .
Thanks everyone
2022-01-24 10:59 PM
Hello have you found a solution? Because I have a similar problem :grinning_face_with_sweat: