cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 while(1) not executed

Angle
Associate II

Hi , may I know why when I put my code under while(1), it doesn't execute my code?

0693W00000Y76snQAB.png

8 REPLIES 8
gbm
Lead III

Look for the reason before the code which is not executed. Use the debugger to catch the problem.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
FBL
ST Employee

Hello @Angle​ 

Could you please provide more details about the product name

Also provide more details on the issue: which MX version are you using? at which level exactly the error is faced?

I suggest to s start with an example using UART.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


Angle
Associate II

Hi, my using the STM32H750XBH-DK touchgfx.

I also don't know why it doesn't execute my code when I put it in while(1) in user begin 3. I think there is no problem with my code since I also try to executed by putting my code at user begin 2 and it working.

0693W00000Y77A8QAJ.png 

This is one is when I put my code in in user begin 2, my code can be executed but I need to add the while(1) since I need to use the loop. I can read the data display

0693W00000Y7790QAB.png 

Angle
Associate II

btw I already start with the very simple basic UART

Doesn't get there due to already having transferred to task started by the scheduler?

P​erhaps stop in the debugger and see what code it IS executing..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AScha.3
Chief III

--- and if you put code in "normal" intended position :

0693W00000Y77MJQAZ.png

If you feel a post has answered your question, please click "Accept as Solution".
gbm
Lead III

So, you skipped few "minor details" from your problem description. The processor never enters the loop, you are starting the operating system scheduler before the loop and the processor is "stuck" in the operating system and the tasks run by it. By definition it should never return from OS start routine.

Can you see the comment "We should never get there as control is now taken by the scheduler"?

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Karl Yamashita
Lead III

You can't use the while loop in main.c as the code never reaches it because the scheduler takes over.

Instead you'll have to use the default task or create a new task in FreeRTOS. But if you use the default task then call some Polling functions in a different file. In main.c you should find a function called StartDefaultTask

/* USER CODE BEGIN Header_StartDefaultTask */
/**
  * @brief  Function implementing the defaultTask thread.
  * @param  argument: Not used
  * @retval None
  */
/* USER CODE END Header_StartDefaultTask */
void StartDefaultTask(void *argument)
{
  /* USER CODE BEGIN 5 */
  /* Infinite loop */
	PollingInit();
  for(;;)
  {
	  PollingRoutine();
    osDelay(0);
  }
  /* USER CODE END 5 */
}

I'm calling PollingInit() that is function that has initializing tasks. This is only called once. Then the PollingRouting() is in the for(;;) loop. So the PollingRoutine is where you'll do you own tasks outside of the TouchGFX tasks.

Tips and Tricks with TimerCallback https://www.youtube.com/@eebykarl
If you find my solution useful, please click the Accept as Solution so others see the solution.