2019-05-21 12:53 AM
Hi everyone,
I've removed the previous, textual guide. Instead, here's a video guide on how to get CubeIDE and TouchGFX working on an STM32F746G-DISCO board. I accidentally exported the video in 720p but have created a 1080p version. Leaving both links here because the 720p version may have useful comments and resolutions:
1080p: https://youtu.be/VOs2LYO7wSA
720p: https://youtu.be/xZ0pPhQCQUY
And here's the project i created and modified:
(NOTE: This project does not have the modifications from our STM32F746G-DISCO/CubeMX article).
Best regards,
Martin
2019-05-27 01:20 AM
@Morgan, i've solved it here. The issue was simply copying "\Middlewares\ST\TouchGFX\touchgfx\framework\source\platform\" into the Library Path settings. If you select the folder through "Add..->Workspace" it should be correct and not cause an error.
2019-05-27 04:09 AM
Please find a working STM32F746G-DISCO project in here:
Working on the script and video tutorial now.
2019-05-27 10:53 PM
Hi Martin,
Even if it's not supported from CubeMX side (which just means that TGFX files are not populated and IDE right configured automatically), it would be nice to have the same kind of working project on L4R9 (ideally + DPI screen) in CubeIDE, as a proven/checked guide.
It would suppose for us manually changes to update gui parts during dev but at least it would be usefull to be sure on the correct files choice and right configuration on this board.
It would be an acceptable solution to wait the full integration at the end of the year.
Thanks.
2019-05-28 06:39 AM
Hi Guys,
I've shot a video of how to get a working STM32F746G-DISCO CubeIDE 1.0 project using TouchGFX 4.10. I won't have time to finish editing (since it's a public company video) until monday next week, probably. But at least it's shot and i just need to put the finishing touches on it.
/Martin
2019-05-29 04:03 AM
I just updated the original post with a video tutorial.
2019-05-29 04:18 AM
I also changed the title of this post to: "STM32CubeIDE and TouchGFX 4.10.0: Resolving compilation issues"
2019-06-03 03:02 AM
Thanks for the video, but unfortunately, I can't read any text on the video (screen resolution 1680x1050). I'll try to watch it at home.
2019-06-04 07:30 AM
I've updated the main post with a 1080p version of the video, which was the intended quality all a long. Sorry for the glitch!
/Martin
2019-06-04 08:31 AM
Thanks Martin! I will check out the new version of the video. I really appreciate it.
2019-06-04 02:11 PM
No problem. Hope it's more useful in this new format - Otherwise i may have to reshoot the whole thing in a lower native resolution.