2019-05-21 12:53 AM
Hi everyone,
I've removed the previous, textual guide. Instead, here's a video guide on how to get CubeIDE and TouchGFX working on an STM32F746G-DISCO board. I accidentally exported the video in 720p but have created a 1080p version. Leaving both links here because the 720p version may have useful comments and resolutions:
1080p: https://youtu.be/VOs2LYO7wSA
720p: https://youtu.be/xZ0pPhQCQUY
And here's the project i created and modified:
(NOTE: This project does not have the modifications from our STM32F746G-DISCO/CubeMX article).
Best regards,
Martin
2019-06-05 6:35 AM
Hello,
Thank you Martin for your 1080p video. I tried to follow it but I have the same problem as last time. When I try to build the project many paths of .hpp files are wrong. The .hpp files exist but the paths are wrong. For example, I get the following error : C:/STM32CubeProject/GenerateurPulse/TouchGFX/gui/include/gui/common/FrontendHeap.hpp:4:10: fatal error: gui_generated/common/FrontendHeapBase.hpp: No such file or directory
So I started add all the paths of the .hpp in "Includes " (Path and symbol window). However it take too much time. Do you think I have a problem with the general properties of CubeIDE ?
Valentin
2019-06-05 9:23 AM
Hi @Valentin Gros ,
I have a problem every time when I generate code in CubeMX, it erases the path configurations and I need to add manually.
Please check your path and symbol window, it needs to be like this (pay attention in excluded paths too):
Regards,
Anderson
2019-06-05 11:31 AM
I would have to agree with you that you may need to reshoot in a lower native resolution because it is still very hard to see. I found myself counting items (and sometimes guessing) to duplicate what you did because I could not read the text.
2019-06-06 12:45 AM
Hi Valentin,
I was affraid this would happen. I have seen this problem on occasion where all the source/include folders for the application itself are not added and then compilation fails. It does not happen always. I will add this to the list of issues with CubeIDE generation internally.
/Martin
2019-06-06 12:47 AM
I was affraid you'd say that :D Okay, thanks for the feedback, Scott!
/Martin
2019-06-06 11:23 PM
Hello eng23,
Thank you for your answer, I will try.
2019-06-06 11:32 PM
Hi guys,
Yes, CubeMX/CubeIDE will overwrite any changes you make, unfortunately. I'll come up with a quick guide to get past this in a less painful way than doing things manually.
This is already reported to CubeMX/IDE team.
/Martin
2019-06-06 11:39 PM
Hello Martin,
My project "pulse generator" is completed. For your information, I used a STM32F746G-DISCO with the working project you gave us and a NUCLEO-STM32F767ZI. Both communicate with serial communication UART. I use the F746G only for graphics (because I can't regenerate code without breaking project) and the F767ZI for pulse generation.
To conclude :
Thank you for all your work !
Valentin
2019-06-07 12:27 AM
Hi Valentin,
Great work! Glad to be of help and sorry for all the trouble :) Appreciate all the feedback - This is great for us to pass on and make the integration between ST tools much smoother than it is.
/Martin
2019-06-07 6:21 AM
Hi Martin
Is there a way to address this for the time being?
I tried using the template code you provided from other post but it keeps giving error of files missing.
https://community.st.com/s/question/0D50X0000ArSsjqSQC/using-hyperram-for-display-buffer-on-stm32l4r9ieval