2019-10-10 4:14 PM
I'm using an stm32f769 on an ARGB8888 system.
I'm creating a bitmap image in RAM from a JPEG using the hardware decoder. This is decode process does NOT set the alpha byte to 0xff so the GUI_DrawBitmap function using the GUI_DRAW_BMP8888 method doesn't display anything (its all transparent).
How do I force STemWin to ignore the alpha channel (or lack of it) so that my image displays.
I've tried GUI_SetAlpha() and GUI_EnableAlpha () in various combinations but to no effect.
2019-10-17 5:49 PM
Further research reveals that neither GUI_SetAlpha or GUI_SetUserAlpha ever calls LCD_X_SETALPHA cmd in the LCD driver so the layer Alpha value never gets updated.
Is it really this broken or am I just lucky?