2021-04-30 8:47 AM
Also some sample code, just to start, may be useful for unserstanding events and how to connect events to the microcontroller state.
2021-05-01 12:50 AM
Examples is in designer start window and latest is 4.16.1
2021-05-03 1:15 AM
Hello Hicsss.2033,
Like MM..1 mentioned, please use TouchGFX 4.16.1 with TouchGFX Designer. You will have many examples and demos.
Also I highly recommend you to read the documentation website.
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2021-05-03 3:35 AM
I'm using system workbench and, for what I have inderstood, it works only with the version 4.10.0. Do the examples that you are citing work also for 4.10.0?
2021-05-03 3:36 AM
Thanks for your answer.
Where can I find the designer start windows? I'm using system workbench which, for what I undestood, is compatible only with 4.10.0.