Hello @Sejinoh If you are satisfied with @Sean Park's answer, please close this request by choosing Select as Best.Feel free to ask other questions on the community in English /Alexandre
Hello @Riccardo Franceschetto Did you try to use TouchGFX without OS and see if the issue still occurs ?If you don't do anything on the display while running the DAC, I believe you should be able to reach 20 KHz.Why TouchGFX is calling the DAC ? Can...
Hello Guopeng,Have you created a dedicated task for the video decoding ?The F769-DK TBS available in TouchGFX Designer supports the video widget out-of-the-box.Please check and make sure that you have the same configuration on your side./Alexandre
Hello BGuth.1,I was able to reproduce your issue.One workaround is to set the value of the slider which forces the slider to refresh itself properly.slider1.setBitmaps(touchgfx::Bitmap(BITMAP_SLIDER_BASE_DARK_ID), touchgfx::Bitmap(BITMAP_SLIDER_BASE...
Hello BGuth.1,Do you confirm that if you use the Designer to configure the base image of your slider, the issue does not appear ?If that's the case, your line of code is probably wrong and you should compare with what TouchGFX generates when configur...