2023-01-25 08:25 AM
Hello,
I'm working on a STM32F769I-Eval demoboard.
I have a FreeRTOS and FreeRTOS-Plus-TCP running on it. I can ping the board with a 100% succes.
When I start a basic TouchGFX 4.21 Application, even without any refresh, the Ping response fall to 30%.
As the TouchGFX as no animation, the refresh rate is not so important. How can I reduce it to avoid the TCP task miss some ping packet?
Or is there any other possibility to reduce MCU consumption by TouchGFX?
Thank you
Antoine
2023-01-25 09:22 AM
Touchgfx mode ? LTDC / Custom Single Double Partial SPI ?...
2023-01-26 12:51 AM
did you not implement a timer etc for genVSync() ? This should control how often the screen is updated
i use an spi display and call this function every 100ms. but only on screen changes the display is really updated. i do not know if this is maybe different with other displays?
2023-01-26 07:18 AM
Interface selected in CubeMX is custom. I do not change anything to the ioc file generated by TouchGFX designer from the board template.
2023-01-26 07:19 AM
Hello,
I do not implement any timer. I'm using the code generated from TouchGFX designer and CubeMX. I will have a look to change the VSync generation timer.
2023-01-26 07:44 AM
The generated code from TouchGFX Designer and CubeMX use a "Custom" interface instead of the "Parallel RGB (LTDC)" interface.
Is it not better to use it? Or is there a reason not to use it?