2022-06-04 08:48 AM
Hi.
I am using a ili9488 display along side with stm32h7b0vbt6.
the lcd driver works fine... but touchgfx wont work.
(FMC bank mapping is swapped.)
first:
"TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect)" function is the only function that should be edited? and how?
I had a look on l496-disco example but it seem it was created by old versions of touchgfx. some codes was different from my project...
second:
is it possible to use the GRAM as frame buffer?
thanks.
2022-06-08 01:18 AM
Hello @SEMad ,
What do you mean exactly with "TouchGFX won't work" ? Is the designer not generating code or is it not running or target ?
And just to be sure, which version of the designer are you using ?
Thank you,
/Yoann