2021-10-25 11:28 PM - last edited on 2024-03-05 6:11 AM by GaetanGodart
I am trying to port a Project using TouchGFX (Designer 4.17) and FreeRTOS to our own RTOS using IAR 8.40 Toolchain and th STM32F769I-Disco Board (Same controller will be used in the final product).
When calling MX_TouchGFX_Init() the System runs into an a HardFault
The HardFault occurs in the Library code (touchgfx::Screen::draw accroding to disassemly PC: 0x3ade9e, calles from touchgfx::Application)
_ZN8touchgfx6Screen4drawEv:
0x3a'de7e: 0xb53e PUSH {R1-R5, LR}
0x3a'de80: 0x2200 MOVS R2, #0
0x3a'de82: 0xf8df 0x4264 LDR.W R4, [PC, #0x264] ; _ZN8touchgfx3HAL13DISPLAY_WIDTHE
touchgfx::HAL::DISPLAY_WIDTH
0x3a'de86: 0x9200 STR R2, [SP]
0x3a'de88: 0xf8df 0x3258 LDR.W R3, [PC, #0x258] ; _ZN8touchgfx3HAL14DISPLAY_HEIGHTE
touchgfx::HAL::DISPLAY_HEIGHT
0x3a'de8c: 0x5ea2 LDRSH R2, [R4, R2]
0x3a'de8e: 0xf9b3 0x5000 LDRSH.W R5, [R3]
0x3a'de92: 0xf8ad 0x2004 STRH.W R2, [SP, #0x4]
0x3a'de96: 0x4669 MOV R1, SP
0x3a'de98: 0xf8ad 0x5006 STRH.W R5, [SP, #0x6]
0x3a'de9c: 0x6802 LDR R2, [R0]
0x3a'de9e: 0x6893 LDR R3, [R2, #0x8]
0x3a'dea0: 0x4798 BLX R3
0x3a'dea2: 0xb003 ADD SP, SP, #0xc
0x3a'dea4: 0xbd30 POP {R4, R5, PC}
As far as I see this i do not have much options to break the
Solved! Go to Solution.
2021-11-03 3:48 AM
Hi,
CRC is necessary to work with TouchGFX Designer and other ST packs. You get a warning message in the X-CUBE-TOUCHGFX.4.18.0 settings within STM32CubeMX when it is not enabled.
/Romain
2021-10-26 3:42 AM
Is your screen empty ? Try start with one screen one box empty project.
2021-10-26 10:54 PM
I do have a version with empty screen. Unfortunately the HardFault does occur also with the empty app
2021-10-27 12:34 AM
What version of TouchGFX are you using ? Could you share your FreeRTOS tasks just to check ? May be completely unrelated but i just want to see if you have named it properly and if the stack size is big enough.
/Romain
2021-10-27 3:28 AM
Add something to screen
2021-10-29 12:43 PM
I have added a green screen. Still the same hardFault
2021-10-29 12:47 PM
I am using version 4.17 of the designer. Is this automatically the version of the lib? or where do I find it?
I do not use FreeRTOS. When I do, the application runs fine.
I have now doubled both stack an heap size (since TouchGFX und Control application on there own are happy with the initial 0x2000), no change
2021-11-02 11:30 PM
Meanwhile. I have found the error. I have not initialized the CRC module but it is used within the library. Maybe it would be worth it to point out that this module is used in a future version of the lib? Thank you for your support
2021-11-03 3:48 AM
Hi,
CRC is necessary to work with TouchGFX Designer and other ST packs. You get a warning message in the X-CUBE-TOUCHGFX.4.18.0 settings within STM32CubeMX when it is not enabled.
/Romain
2024-03-01 8:56 AM
You get a warning when it's not enabled, but not a warning when "Do Not Generate Function Call" is checked. And I assume also no error if it is initialized after TouchGFX. In our code we had hardfaults and got no warnings because of this. Thank you MMenz.1 for giving your solution!