Hi all,I have setup the demo project with the P-NUCLEO-IHM03 and I can start the motor using the Motor Pilot 6.2.1. So far so good. Since I want to use a stronger Motor eventually, I have bought the IHM-08 and want to use it with the Gimbal Motor as ...