2025-03-12 2:57 PM
Hi all
I'm struggling for a while getting a µSD Card to run via SDMMC on FileX. I'm using a Nucleo U575 Board with an external SDMMC/SDIO-breakout board. I tried to follow the "Fx_uSD_File_Edit" example for the U575I-EV board.
Long story short, I set up a FileX application thread on ThreadX and I'm trying to just open the media.
In main.c there's the automatically generated MX_SDMMC1_SD_Init() initializing the the SDMMC1 interface just after GPIOs and ICACHE were initialized. In main.c everything runs through without any error.
However, when entering the FileX application, the very first function getting called is MX_SDMMC1_SD_Init() again - as I configured FileX to initialize the SD IP (just as seen in the Fx_uSD_File_Edit-example). This time it ends in a HardFault in the Init. The one thing that I really don't understand is that it happens just on the call of
sdmmc_clk = HAL_RCCEx_GetPeriphCLKFreq(RCC_PERIPHCLK_SDMMC);in stm32u5xx_hal_sd.c
I enabled a breakpoint on the very first line of HAL_RCCEx_GetPeriphCLKFreq. The first time (called from inside main.c) it runs through flawlessly as stated above. But on the second call (from fx_stm32_sd_driver_glue.c) it doesn't even stop at the breakpoint but just going to a HardFault.
Can anyone explain this problem or try to give me a hint on how to fix this issue?
Best
M
Solved! Go to Solution.
2025-06-22 8:21 AM
I was able to fix the problem! In fact there were 2 problems:
1. The example didn't run as there is exFAT support deactivated by default. activating it made it run with my µSD cards laying around - or formatting one of which to FAT32.
2. In my own code, the stack size configured for the FileX-Thread was too small. I guess I need to take a class on how to elaborate what stack sizes, memory pool sizes etc. to choose for the single threads.
2025-03-18 2:56 AM
Hello @MGuth.1
Please refer to article How to use FileX with eMMC for file system management for detailed steps to set your project.
2025-03-24 2:51 PM
Hi Omar
Thanks for your answer and the attached How-to. I sticked to the guide as good as possible, choosing the SDMMC interface instead of the MMC interface. Also I didn't use LevelX as it doesn't have an option for SDMMC (or should I choose for NAND here?).
However, I'm still getting a HardFault when trying to open the media through
fx_media_open()
[...] -->
(media_ptr -> fx_media_driver_entry) (media_ptr)
[...] -->
if (SDMMC_GetCommandResponse()). Again I'm jumping to the HardFault Handler just when calling the SDMMC_GetCommandResponse() without any hint on the reason...
Any guesses what could be the reason for the failure?
Thanks in advance.
2025-03-26 1:31 PM - edited 2025-03-26 1:38 PM
This is the point where the HardFault occurs. With the data given on the right (collapsed structures only hold zeros), hitting "Step Into" it goes directly into the Hard Fault.
SDMMC_GetCommandResponse just returns SDMMCx-->RESPCMD which equals SD_CMD. So the if-statement in line 1395 should be skipped and the programm should continue at line 1401. But when setting a breakpoint on 1401, it goes to the HardFault just as said above.
Does this help to narrow down the problem in any way?
2025-03-28 3:46 AM
Hello @MGuth.1
Could you try to communicate with uSD directly with HAL and without FileX please?
You can refer to this example Projects/STM32U575I-EV/Examples/SD/SD_ReadWrite_DMALinkedList.
2025-03-28 7:57 AM
Hi @Saket_Om
Thanks for your continuous input and help.
I just downloaded the example you linked to. I loaded it to my Nucleo U575 board without touching the external SD-breakout board (same connection as for the initial program). The example runs through without any problems. When inserting the µSD Card to my Computer afterwards I see it was formatted - or at least renamed.
So the basis, HAL-interface, seems to be working just fine. I assume this narrows the problem down to a configuration issue for FileX ?!
2025-04-02 12:47 AM
Hello @MGuth.1
Please try adding fileX and check if it works. Once it does, try adding ThreadX.
Please look to this example as reference "Projects/STM32U575I-EV/Applications/FileX/Fx_File_Edit_Standalone"
2025-05-12 11:55 AM
Hi @Saket_Om
Thanks for staying with me. It took some time for me to work on the topic again.Unfortunately I'm stuck at adding fileX.
As checked previously, HAL seems to be working fine with the SD card: I can write blocks and also read data to/from the µSD card. When adding fileX, I get the same error as described in the original post. Meanwhile I also tried to eliminate doubts in hardware mistakes: I tried with several µSD cards (different brands and models, from cheap ones to SanDisk, Samsung, Kingston), cardholders (breakout boards, different models), re-wired everything... Unfortunately I wasn't able to get it running using fileX.
As far as I understand the example you mentioned above ("U575I-EV/.../Fx_File_Edit_Standalone") should run on my Nucleo U575 board without any code changes?!
Is there any crucial setting for the sd card that I'm missing? Like minimum SD-card standard/class, maximum storage size of the card, etc?
Best regards
Matthias
2025-06-22 8:21 AM
I was able to fix the problem! In fact there were 2 problems:
1. The example didn't run as there is exFAT support deactivated by default. activating it made it run with my µSD cards laying around - or formatting one of which to FAT32.
2. In my own code, the stack size configured for the FileX-Thread was too small. I guess I need to take a class on how to elaborate what stack sizes, memory pool sizes etc. to choose for the single threads.