cancel
Showing results for 
Search instead for 
Did you mean: 

What is up with STM32H563 ADC INP0?

Dimlite
Associate III

Hi,

I am not able to get a correct reading from ADC1 INP0 (PA0). All the other analog channels works fine.


The datasheet mentions this:

ADC option register (ADC_OR), option bit 0 (OP0)

For ADC1:

0: INP0/INN1 GPIO switch control disabled

1: INP0/INN1 GPIO switch control enabled

Note:This option bit must be set to 1 when ADCx_INP0 or ADCx_INN1 channel is selected.


The expected value is 2048, but I get 4095 when OP = 1, and 3433 with OP0.

The input has a 2 k resistor in series, and I measure 1.5 V (correct) on the far side, and 1.3 V on the side directly connected to the input.


Please see attached file, which is from the datasheet for RGT6. I don't know how to interpret the table. Is option register implemented or not regarding ADC1?


What is the purpose of the option bit, and what am I missing here?

4 REPLIES 4
Andrew Neil
Evangelist III

It is a custom board.

Though I doubt this is related to the external HW, please see attached file.The schematic consists of multiple pages that I can not share. To the right you see the LP-filter mentioned above (2k + cap). This is connected to PA0, though not on this page.