cancel
Showing results for 
Search instead for 
Did you mean: 

What are the pins are Slow, Fast and Direct ADC channels in STM32H7A3VIT6 MCUs?

HChan.7
Associate II
 
2 REPLIES 2
HChan.7
Associate II

As per Data Sheet, (DS13195 or STM32H7AxI/G datasheet)

Direct channels are connected to analog I/Os (PA0_C, PA1_C, PC2_C and PC3_C)

Fast channels correspond for ADCx_INPx to PA6, PB1, PC4, PF11, PF13 and for ADCx_INNx to PA7, PB0,PC5, PF12, PF14

I could not able to find the PA0_C. PA1_C and PF11, PF12, PF13 and PF14 pins in STM32H7A3VIT6 pinout.

Could you please help me for this?

TDK
Guru

Not all chips have all pins broken out.

The STM32H7A3VIT6 is a LQFP100.

Looking at the datasheet, you can see that the PA0_C isn't broken out on this package. Same for the other pins you are looking for.

0693W00000KZccXQAT.png

If you feel a post has answered your question, please click "Accept as Solution".