cancel
Showing results for 
Search instead for 
Did you mean: 

Wait but MCU is unblocked

XooM
Senior

I haven't been able to wait 500ms without affecting the timers for 7 days.
In this block, doesn't PB14 become "0" after 500ms?
Even if I use comment lines, it doesn't work.

Note: volatile uint32_t Counter = 0;
The "Counter" variable is incremented every 1ms with Timer16.

 

** STM32F030C6T6 I'm using.

** Own PCB board..

*** Note: Card of a working system.. There is no card design error.

 

 

if(htim->Instance==TIM16) { Counter++; if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)==0) { if(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_2)==0) { if(PA10_On==0) { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET); HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14,GPIO_PIN_SET); Counter=0; PA10_On=1; // Tick_PA10_On= HAL_GetTick(); // PA10_On=1; } else { if(Counter>500) // if((HAL_GetTick()-Tick_PA10_On)>=500) { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14,GPIO_PIN_RESET); Counter=501; } } } else { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_SET); } } else { HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET); } }
View more

 

 

60 REPLIES 60

I think the problem is that the Hal_delay function is not working. But I still haven't found the solution.


@XooM wrote:

I think the problem is that the Hal_delay function is not working. But I still haven't found the solution.


If you tell me your board, MCU and STM32CubeMX version I can check. Hal_delay works perfectly fine in my projects. I cannot replicate your situation if I don't know the details.

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

XooM_0-1732013256689.png

STM32F030C6T6 i'm using.

I am not using ST board.
A custom designed PCB..
Removed from a working machine..
I can't write code because I got stuck while reprogramming.

@XooM wrote:

I can't write code because I got stuck while reprogramming.


You cannot FLASH the MCU? What programmer are you using? And at what bitrate?


@XooM wrote:
The program is starting to go crazy.

Can you clarify?

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

Hayır, programlayabilirim. Şimdi sıkışıp kaldım çünkü kızgınım.

ST-LINK V2 orijinal.

Does your board contain an LED?
Have you tried to make a blinky?

Can you send your ioc file?

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.
 

XooM_0-1732015665310.png

PA10 is SET but not RESET. It remains stuck in the SET position.

unsigned_char_array_1-1732015972986.png

Please give pins functional names. It makes it easier to use it in code using the generated defines in main.h:

#define YOURPINNAME_Pin GPIO_PIN_14 #define YOURPINNAME_GPIO_Port GPIOB

I noticed pin PINB12 and PINC13 referenced in your start post are missing in the configuration. Please configure all iopins

Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

I'll take care of them, so why isn't Hal_delay working?
My problem is exactly that the hal_delay function isn't working.
I didn't care about the names because I was writing a test program.