2024-01-23 12:00 AM
Hi, I have STM32F103 and STM32F411. I have successfully made HID mouse on STM32F103, but when I try to make the same on STM32F411, the mouse does not work: "(Code 43) A request for the USB device descriptor failed".
What could be the problem?
The code/configuration is simple I just enable:
Connectivity -> USB_OTG_FS -> Mode: Device_Only
Middleware -> USB_DEVICE -> Class for FS IP: Human Interface Device class (HID)
Everything else is kept default.
Is this because STM32F103 has micro USB and STM32F411 has type-c? Does type-c need additional settings which I am missing?
Solved! Go to Solution.
2024-01-23 3:23 AM
Nevermind... It seems that I set wrong oscillator value... 16Mhz instead of 25Mhz! Now mouse example is working!
2024-01-23 12:29 AM
Hi,
> Is this because STM32F103 has micro USB and STM32F411 has type-c?
No, the message tells you: "..USB device descriptor failed".
So look in your F103 project, what is missing in F411 project (-- device descriptor ) .
2024-01-23 2:05 AM
I don't think I have changed anything manually. Everything should be kept as default after generating the project with CubeMX.
2024-01-23 3:23 AM
Nevermind... It seems that I set wrong oscillator value... 16Mhz instead of 25Mhz! Now mouse example is working!
2024-01-23 3:30 AM
@JBond.1 wrote:I don't think I have changed anything manually. Everything should be kept as default
But defaults could be different between F103 and F411 ... ?
2024-01-23 3:48 AM
The issue was in wrong clock configuration. Oscillator value 16Mhz instead of 25Mhz.