2024-09-11 10:24 AM - last edited on 2024-09-16 8:09 AM by mƎALLEm
Hello, so I am completely new to working with STM boards in general.
I just got a brand new stm32f446re board, and I tried to upload some code to it through Linux. And I do mean brand new, I haven't uploaded or downloaded any code to it before this attempt. However, when I attempted to do so, I got an error message:
"WARN common.c: unknown chip id! 0x421"
So, I looked around for a bit and tried a simple command: st-info --probe to see some internal stuff on it. But I was told this:
"No such file or directory
version:V2J33S25
serial: 066DFF534871754867255336
flash: 0 (pagesize: 0)
sram: 0
chipid: 0x421"
After spending roughly about two weeks trying to find stuff online, I couldn't figure out anything on what to do. So, I am very much open to suggestions if anybody knows anything about this error.
Thank you very much in advance for any help.
Solved! Go to Solution.
2024-09-16 9:21 AM
@Andrew Neil wrote:
@waclawek.jan wrote:I maintain that those utilities are of an obsolete version and/or incorrectly installed.
Plausible - and that was also @Tesla DeLorean's feeling, I think.
https://github.com/stlink-org/stlink/issues/1241#issuecomment-1366964332
As already noted, it's a 3rd-party project - so you need to take issues up with them.
2024-09-11 10:30 AM
@Odega wrote:I am completely new to working with STM boards in general. .
Do you have experience with any other microcontroller(s)? With programming in general? Electronics?
@Odega wrote:I just got a brand new stm32f446re board
What board, exactly - ST? 3rd-party? custom?
What, exactly, are you using to do the downloading?
2024-09-11 10:32 AM
Hello @Odega and welcome to the community,
@Odega wrote:
I just got a brand new stm32f446re board, and I tried to upload some code to it through Linux. And I do mean brand new, I haven't uploaded or downloaded any code to it before this attempt. .
What tool are you using to connect to the board?
What board are you using? NUCLEO-F446RE?
2024-09-11 10:37 AM
Thank you for the welcome to the community.
I am using a Nucleo-F446RE.
And to connect to the board I am just using a USB cord to connect to said board. Beyond that, I am just using the Terminal that came with the laptop I was given.
2024-09-11 10:41 AM
So what software tools are you using to download the code to the board?
And what code are you trying to download?
You didn't answer about your background/experience - that would help in knowing how to pitch replies...
2024-09-11 10:42 AM
I am an electrical engineering student, so I have some basic experience with Stm32 boards, but nothing overly expansive. I've used keil to program one before, and know some C and Python programming languages.
I'm just working with an stm32 nucleo f446re. And I am just using a USB cord. I have been told that for this specific code that I am working with, I was told that using a USB has worked in the past and to just do that.
Thank you for that link btw. I'm completely new to writing on message boards like this so I didn't know any of that.
2024-09-11 10:46 AM
And for the record, I am just compiling the code on Linux (I don't know the specifics of the version of Linux or anything). I'm uploading a compiled set of code that was pre-written before I ever joined this project. But from what I have been told, the overall code portion shouldn't matter.
I got this new board because a previous one was having connection issues with the laptop I am working on, so I was hoping that the new board would work right off the bat. Should have known it is never just that easy.
2024-09-11 10:56 AM
Some old/broken tools..
case 0x421 : printf("STM32F446\n"); break; // Been known here for a while..
2024-09-12 2:00 AM
Hello @Odega ,
You still didn't provide what tool you are using to compile the project and to upload it to the MCU.
Example for ST tools:
- STM32CubeIDE: to compile/uploaded and debug available on Linux platform.
- STM32CubeProgrammer: to manipulate the internal/enteral Flash and option bytes.
- On board ST-LINK: as in-circuit debugger and programmer to connect and upload you program to the MCU. USB data cable needs to be connected on CN1 as indicated by the red rectangle.
2024-09-16 7:48 AM
What I am using to compile the code is Ubuntu Linux. Beyond that and typing up a simple list of commands, I don't use any external tools. I wanted to try CubeProgrammer but I could never get it to work on Ubuntu.
Apologies for the delayed response.